NodesBetweenNodesBuilder Class¶
-
class
NXOpen.CAE.
NodesBetweenNodesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodesBetweenNodesBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodesBetweenNodesBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Increment | Returns or sets the increment |
Label | Returns or sets the label |
Node | Returns the node |
NumNodes | Returns or sets the num nodes |
Tag | Returns the Tag for this object. |
Type | Returns or sets the node creation type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedNodes | The last created nodes |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NodesBetweenNodesBuilderTypeEnum Enumeration | the method of creation of node |
Property Detail¶
Increment¶
-
NodesBetweenNodesBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment
Parameters: increment (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
NodesBetweenNodesBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
NodesBetweenNodesBuilder.
Node
¶ Returns the node
-------------------------------------
Getter Method
Signature
Node
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX5.0.0.
License requirements: None.
NumNodes¶
-
NodesBetweenNodesBuilder.
NumNodes
¶ Returns or sets the num nodes
-------------------------------------
Getter Method
Signature
NumNodes
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumNodes
Parameters: numNodes (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Type¶
-
NodesBetweenNodesBuilder.
Type
¶ Returns or sets the node creation type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.CAE.NodesBetweenNodesBuilderTypeEnum
New in version NX7.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: nodeCreationType ( NXOpen.CAE.NodesBetweenNodesBuilderTypeEnum
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetCommittedNodes¶
-
NodesBetweenNodesBuilder.
GetCommittedNodes
¶ The last created nodes
Signature
GetCommittedNodes()
Returns: Return type: list of NXOpen.CAE.FENode
New in version NX7.5.1.
License requirements: None.
Validate¶
-
NodesBetweenNodesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.