NodeTranslateBuilderMethodType Enumeration

NXOpen.CAE.NodeTranslateBuilder.MethodType is an alias for NXOpen.CAE.NodeTranslateBuilderMethodType

class NXOpen.CAE.NodeTranslateBuilderMethodType

Bases: object

the method types

Enum Members

Enum Member Enum Member Description
ByComponents by components
AlongDirection along direction
AlignVectors align vectors
PointToPoint point to point
ScaleModel scale model
ByField by field
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.