NodeRotateBuilderCopyType Enumeration

NXOpen.CAE.NodeRotateBuilder.CopyType is an alias for NXOpen.CAE.NodeRotateBuilderCopyType

class NXOpen.CAE.NodeRotateBuilderCopyType

Bases: object

the copy types

Enum Members

Enum Member Enum Member Description
RotateOnly rotate only
CopyRotate copy rotate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.