MorphRevolvedMeshBuilder Class¶
-
class
NXOpen.CAE.
MorphRevolvedMeshBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.MorphRevolvedMeshBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateMorphRevolvedMeshBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Axis | Returns or sets the axis of revolution |
Elements | Returns the elements |
FixedNodes | Returns the fixed nodes |
SourceNodes | Returns the source nodes |
Tag | Returns the Tag for this object. |
TargetCurveType | Returns or sets the curve type |
TargetCurves | Returns the curve |
TargetLineEnd | Returns or sets the line end |
TargetLineStart | Returns or sets the line start |
Methods¶
Method | Description |
---|---|
AddOrModifyNodeMap | Add or modify node to point mapping |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetNodeMappedPoint | Get point mapped to the given node |
GetObject | Returns the object currently being edited by this builder. |
RemoveNodeMap | Remove node from node to point mapping |
ReplaceNodeMap | Replace old node mapping with new node to point mapping |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MorphRevolvedMeshBuilderCurveType Enumeration | the type of curve to be used as reference curve for morphing |
Property Detail¶
Axis¶
-
MorphRevolvedMeshBuilder.
Axis
¶ Returns or sets the axis of revolution
-------------------------------------
Getter Method
Signature
Axis
Returns: Return type: NXOpen.Axis
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis
Parameters: axis ( NXOpen.Axis
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
MorphRevolvedMeshBuilder.
Elements
¶ Returns the elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX11.0.0.
License requirements: None.
FixedNodes¶
-
MorphRevolvedMeshBuilder.
FixedNodes
¶ Returns the fixed nodes
-------------------------------------
Getter Method
Signature
FixedNodes
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX11.0.0.
License requirements: None.
SourceNodes¶
-
MorphRevolvedMeshBuilder.
SourceNodes
¶ Returns the source nodes
-------------------------------------
Getter Method
Signature
SourceNodes
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX11.0.0.
License requirements: None.
TargetCurveType¶
-
MorphRevolvedMeshBuilder.
TargetCurveType
¶ Returns or sets the curve type
-------------------------------------
Getter Method
Signature
TargetCurveType
Returns: Return type: NXOpen.CAE.MorphRevolvedMeshBuilderCurveType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetCurveType
Parameters: targetCurveType ( NXOpen.CAE.MorphRevolvedMeshBuilderCurveType
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetCurves¶
-
MorphRevolvedMeshBuilder.
TargetCurves
¶ Returns the curve
-------------------------------------
Getter Method
Signature
TargetCurves
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
TargetLineEnd¶
-
MorphRevolvedMeshBuilder.
TargetLineEnd
¶ Returns or sets the line end
-------------------------------------
Getter Method
Signature
TargetLineEnd
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetLineEnd
Parameters: targetLineEnd ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetLineStart¶
-
MorphRevolvedMeshBuilder.
TargetLineStart
¶ Returns or sets the line start
-------------------------------------
Getter Method
Signature
TargetLineStart
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetLineStart
Parameters: targetLineStart ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
AddOrModifyNodeMap¶
-
MorphRevolvedMeshBuilder.
AddOrModifyNodeMap
¶ Add or modify node to point mapping
Signature
AddOrModifyNodeMap(node, point)
Parameters: - node (
NXOpen.CAE.FENode
) – - point (
NXOpen.Point
) –
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- node (
GetNodeMappedPoint¶
-
MorphRevolvedMeshBuilder.
GetNodeMappedPoint
¶ Get point mapped to the given node
Signature
GetNodeMappedPoint(node)
Parameters: node ( NXOpen.CAE.FENode
) –Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
RemoveNodeMap¶
-
MorphRevolvedMeshBuilder.
RemoveNodeMap
¶ Remove node from node to point mapping
Signature
RemoveNodeMap(node)
Parameters: node ( NXOpen.CAE.FENode
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReplaceNodeMap¶
-
MorphRevolvedMeshBuilder.
ReplaceNodeMap
¶ Replace old node mapping with new node to point mapping
Signature
ReplaceNodeMap(oldNode, newNode, newPoint)
Parameters: - oldNode (
NXOpen.CAE.FENode
) – - newNode (
NXOpen.CAE.FENode
) – - newPoint (
NXOpen.Point
) –
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- oldNode (
Validate¶
-
MorphRevolvedMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.