ModelUpdateDesignVariablesRapidCreateBuilderMaterialTypesEnum Enumeration

NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilder.MaterialTypesEnum is an alias for NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderMaterialTypesEnum

class NXOpen.CAE.ModelUpdateDesignVariablesRapidCreateBuilderMaterialTypesEnum

Bases: object

The enum for the material type.

Enum Members

Enum Member Enum Member Description
Mat1
Mat2
Mat3
Mat8
Mat9
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.