ModelDisplayBuilderRotationAxisLineFont Enumeration¶
NXOpen.CAE.ModelDisplayBuilder.RotationAxisLineFont is an alias for NXOpen.CAE.ModelDisplayBuilderRotationAxisLineFont
-
class
NXOpen.CAE.
ModelDisplayBuilderRotationAxisLineFont
¶ Bases:
object
specifies the object font for model rotation axis
New in version NX11.0.0.
Enum Members
Enum Member Enum Member Description Solid Solid font Dashed Dashed font Phantom Phantom font Centerline Centerline font Dotted Dotted font LongDashed Long dashed font DottedDashed Dotted dashed font -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-