ModelDisplayBuilderNodeDisplayModeType Enumeration¶
NXOpen.CAE.ModelDisplayBuilder.NodeDisplayModeType is an alias for NXOpen.CAE.ModelDisplayBuilderNodeDisplayModeType
-
class
NXOpen.CAE.
ModelDisplayBuilderNodeDisplayModeType
¶ Bases:
object
Indicates node display mode type.
Enum Members
Enum Member Enum Member Description Implicit Nodes are implicitly shown according to the following rules. Nodes attached to elements are shown when the elements are shown. Unattached nodes are always shown. Explicit Nodes are explicitly shown and hidden via the Show/Hide commands. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-