ModelDisplayBuilderFreeEdgeMarker Enumeration¶
NXOpen.CAE.ModelDisplayBuilder.FreeEdgeMarker is an alias for NXOpen.CAE.ModelDisplayBuilderFreeEdgeMarker
-
class
NXOpen.CAE.
ModelDisplayBuilderFreeEdgeMarker
¶ Bases:
object
specifies the marker for endpoints of geometry free edges
New in version NX7.5.2.
Enum Members
Enum Member Enum Member Description NotSet No marker Plus Plus marker Dot Dot marker Asterisk Asterisk marker Circle Circle marker Poundsign Pound sign marker Cross Cross marker Square Square marker Triangle Triangle marker Diamond Diamond marker CenterLine Center line marker -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-