AlignBeamElementDirectionBuilder Class |
Represents a NXOpen.CAE.ModelCheck.AlignBeamElementDirectionBuilder builder used to align the Directions of connected beam elements with a seed beam element. |
AlignShellElementFirstEdgeBuilder Class |
Represents a NXOpen.CAE.ModelCheck.AlignShellElementFirstEdgeBuilder builder used to align the first edges of connected shell elements with a seed element edge. |
AlignShellElementNormalBuilder Class |
Represents a NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder builder used to align the normals of connected shell elements with a seed shell element. |
DuplicateElementsCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder to check for duplicate elements within the candidate elements. |
DuplicateNodesCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder to check for duplicate nodes within the candidate nodes. |
ElementEdgeCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder which can be used to detect free element edges or non-manifold edges. |
ElementMaterialOrientationCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder used to check the material orientation for shell and solid elements. |
ElementQualityCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder to perform quality checking on the candidate elements. |
ElementQualityCheckResults Class |
Represents the element quality checking result of NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder |
ElementQualitySetting Class |
|
ElementQualitySettingCollection Class |
Represents a collection of NXOpen.CAE.ModelCheck.ElementQualitySetting in a cae part. |
ElementSpecificTestValue Class |
Represents the quality setting for a specfied element reference
|
ElementTestResult Class |
Represents quality checking result for an element. |
FaceClearanceCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.FaceClearanceCheckBuilder to perform polygon face interference or clearance check. |
ISelectionBuilder Class |
Represents the model check selection builder
|
ITestValue Class |
Represents the quality check criteria value settings
|
ModelSetupCheckBuilder Class |
Represents a NXOpen.CAE.ModelCheck.ModelSetupCheckBuilder which can be used to check if the active NXOpen.CAE.SimSolution contains all the necessary items for the analysis, including elements, loads, constraints and materials. |
QualityTestValue Class |
Represents quality test settings of a specified test type
|
ReverseBeamElementDirectionBuilder Class |
Represents a NXOpen.CAE.ModelCheck.ReverseBeamElementDirectionBuilder used to reverse directions for specified beam elements. |
ReverseShellElementNormalBuilder Class |
Represents a NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder used to reverse normals for specified shell elements. |
SolidElementFaceNormalBuilder Class |
Represents a NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder used to reorient normals for left handed solid elements. |
TestResult Class |
Represents quality checking result of a quality test |
TestValueTypes Class |
Represents the quality check criteria value settings
|