TestValueTypesCriteriaType Enumeration¶
NXOpen.CAE.ModelCheck.TestValueTypes.CriteriaType is an alias for NXOpen.CAE.ModelCheck.TestValueTypesCriteriaType
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesCriteriaType
¶ Bases:
object
the alert level of a criteria value
Enum Members
Enum Member Enum Member Description Warning reports as warning if the check result failed with the criteria value Error reports as error if the check result failed with the criteria value -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-