ElementQualitySettingLimitValue Enumeration¶
NXOpen.CAE.ModelCheck.ElementQualitySetting.LimitValue is an alias for NXOpen.CAE.ModelCheck.ElementQualitySettingLimitValue
-
class
NXOpen.CAE.ModelCheck.
ElementQualitySettingLimitValue
¶ Bases:
object
indicates how criteria value is defined
Enum Members
Enum Member Enum Member Description WarningAndErrorLimit Both warning and error criteria value could be defined ErrorLimitOnly Only error criteria value could be defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-