ElementQualitySettingCollection Class¶
-
class
NXOpen.CAE.ModelCheck.
ElementQualitySettingCollection
¶ Bases:
object
Represents a collection of
NXOpen.CAE.ModelCheck.ElementQualitySetting
in a cae part.To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.CAE.ModelCheck.ElementQualitySetting with the given identifier as recorded in a journal. |
GetElementQualitySetting | Retuns the NXOpen.CAE.ModelCheck.ElementQualitySetting of a specified solver. |
Method Detail¶
FindObject¶
-
ElementQualitySettingCollection.
FindObject
¶ Finds the
NXOpen.CAE.ModelCheck.ElementQualitySetting
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Returns: Return type: NXOpen.CAE.ModelCheck.ElementQualitySetting
New in version NX8.5.0.
License requirements: None.
GetElementQualitySetting¶
-
ElementQualitySettingCollection.
GetElementQualitySetting
¶ Retuns the
NXOpen.CAE.ModelCheck.ElementQualitySetting
of a specified solver.Signature
GetElementQualitySetting(solverName)
Parameters: solverName (str) – Returns: Return type: NXOpen.CAE.ModelCheck.ElementQualitySetting
New in version NX8.5.0.
License requirements: None.