ElementEdgeCheckBuilderScope Enumeration¶
NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder.Scope is an alias for NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderScope
-
class
NXOpen.CAE.ModelCheck.
ElementEdgeCheckBuilderScope
¶ Bases:
object
the Scope over which the Computation of free/non-manifold edges with be done
Enum Members
Enum Member Enum Member Description EntireModel Takes all elements in the model into account while computing VisibleModel Only takes visible elements into account while computing SelectedModels Only takes selected elements into account while computing -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-