DuplicateNodesCheckBuilderMergePreference Enumeration¶
NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder.MergePreference is an alias for NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilderMergePreference
-
class
NXOpen.CAE.ModelCheck.
DuplicateNodesCheckBuilderMergePreference
¶ Bases:
object
Represents the duplicate nodes merging preference
Enum Members
Enum Member Enum Member Description NotSet No preference KeepHighLabel Keep the nodes with higher labels KeepLowLabel Keep the nodes with lower labels KeepSelected Keep the nodes specified in the node list NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder.SelectPreferenceNodesList()
RemoveSelected Merge the nodes specified in the node list NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder.SelectPreferenceNodesList()
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-