DuplicateElementsCheckBuilderDeletePreference Enumeration¶
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.DeletePreference is an alias for NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDeletePreference
-
class
NXOpen.CAE.ModelCheck.
DuplicateElementsCheckBuilderDeletePreference
¶ Bases:
object
Represents the duplicate elements deleting preference
Enum Members
Enum Member Enum Member Description KeepHighLabel Keep the elements with higher labels KeepLowLabel Keep the elements with lower labels KeepSelected Keep the elements specified in the element list NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.PreferenceElements()
RemoveSelected Delete the elements specified in the element list NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.PreferenceElements()
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-