CheckScope Enumeration¶
-
class
NXOpen.CAE.ModelCheck.
CheckScope
¶ Bases:
object
the option indicates the check scope for a model check command Enum Members
Enum Member Enum Member Description Displayed check all displayed elements or nodes Selected check selected elements or nodes -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-