AlignShellElementFirstEdgeBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
AlignShellElementFirstEdgeBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.AlignShellElementFirstEdgeBuilder
builder used to align the first edges of connected shell elements with a seed element edge.To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateAlignShellElementFirstEdgeBuilder()
Default values.
Property Value ElemSelectionMethod ConnectedElementsinSeedMesh New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Direction | Returns or sets the direction |
ElemSelectionMethod | Returns or sets the element selection method |
Elements | Returns the elements |
SeedEdge | Returns the seed edge |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayFirstEdges | Display first edges for connected elements, which are to be aligned with seed edge |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AlignShellElementFirstEdgeBuilderElemSelectionMode Enumeration | the options to define the connection scope to the seed element for model checking |
Property Detail¶
Direction¶
-
AlignShellElementFirstEdgeBuilder.
Direction
¶ Returns or sets the direction
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction (bool) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElemSelectionMethod¶
-
AlignShellElementFirstEdgeBuilder.
ElemSelectionMethod
¶ Returns or sets the element selection method
-------------------------------------
Getter Method
Signature
ElemSelectionMethod
Returns: Return type: NXOpen.CAE.ModelCheck.AlignShellElementFirstEdgeBuilderElemSelectionMode
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElemSelectionMethod
Parameters: elemSelectionMethod ( NXOpen.CAE.ModelCheck.AlignShellElementFirstEdgeBuilderElemSelectionMode
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
AlignShellElementFirstEdgeBuilder.
Elements
¶ Returns the elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX12.0.0.
License requirements: None.
SeedEdge¶
-
AlignShellElementFirstEdgeBuilder.
SeedEdge
¶ Returns the seed edge
-------------------------------------
Getter Method
Signature
SeedEdge
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX12.0.0.
License requirements: None.
Method Detail¶
DisplayFirstEdges¶
-
AlignShellElementFirstEdgeBuilder.
DisplayFirstEdges
¶ Display first edges for connected elements, which are to be aligned with seed edge
Signature
DisplayFirstEdges()
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
AlignShellElementFirstEdgeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.