AlignBeamElementDirectionBuilderConnectedElementScope Enumeration¶
NXOpen.CAE.ModelCheck.AlignBeamElementDirectionBuilder.ConnectedElementScope is an alias for NXOpen.CAE.ModelCheck.AlignBeamElementDirectionBuilderConnectedElementScope
-
class
NXOpen.CAE.ModelCheck.
AlignBeamElementDirectionBuilderConnectedElementScope
¶ Bases:
object
the options to define the connection scope to the seed element for model checking
Enum Members
Enum Member Enum Member Description SeedMesh Limits check to only those beam elements in the mesh that contains the Seed Element AllVisible Limits check to only those beam elements which are connected to the Seed Element and are currently visible UserSpecified Limits check to only those beam elements specified in NXOpen.CAE.ModelCheck.AlignBeamElementDirectionBuilder.UserSpecifiedConnectElements()
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-