MeshControlBuilderWeldSide Enumeration

NXOpen.CAE.MeshControlBuilder.WeldSide is an alias for NXOpen.CAE.MeshControlBuilderWeldSide

class NXOpen.CAE.MeshControlBuilderWeldSide

Bases: object

the mesh control weld row direction subtypes.

Enum Members

Enum Member Enum Member Description
Both
Side1
Side2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.