MeshControlBuilderSizeTypes Enumeration

NXOpen.CAE.MeshControlBuilder.SizeTypes is an alias for NXOpen.CAE.MeshControlBuilderSizeTypes

class NXOpen.CAE.MeshControlBuilderSizeTypes

Bases: object

the mesh control size subtypes.

Enum Members

Enum Member Enum Member Description
All
Start
End
StartAndEnd
LastValue
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.