MeshControlBuilderProgressionTypes Enumeration

NXOpen.CAE.MeshControlBuilder.ProgressionTypes is an alias for NXOpen.CAE.MeshControlBuilderProgressionTypes

class NXOpen.CAE.MeshControlBuilderProgressionTypes

Bases: object

the mesh control progression subtypes.

Enum Members

Enum Member Enum Member Description
Start
End
Center
LastValue
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.