MeshControlBuilderHeightDefinedByOption Enumeration

NXOpen.CAE.MeshControlBuilder.HeightDefinedByOption is an alias for NXOpen.CAE.MeshControlBuilderHeightDefinedByOption

class NXOpen.CAE.MeshControlBuilderHeightDefinedByOption

Bases: object

the height defined by options.

Enum Members

Enum Member Enum Member Description
TotalThickness
GrowthRate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.