MeshControlBuilderCylinderAxialElementSizeType Enumeration¶
NXOpen.CAE.MeshControlBuilder.CylinderAxialElementSizeType is an alias for NXOpen.CAE.MeshControlBuilderCylinderAxialElementSizeType
-
class
NXOpen.CAE.
MeshControlBuilderCylinderAxialElementSizeType
¶ Bases:
object
the cylinder subtypes for size on axial direction.
Enum Members
Enum Member Enum Member Description NotSet Number Size -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-