ManualMorphBuilderMapType Enumeration¶
NXOpen.CAE.ManualMorphBuilder.MapType is an alias for NXOpen.CAE.ManualMorphBuilderMapType
-
class
NXOpen.CAE.
ManualMorphBuilderMapType
¶ Bases:
object
Represents the type of Manual Mapping
Enum Members
Enum Member Enum Member Description Stationary stationary mapping NodeToPoint node to point mapping NodeToEdge node to edge mapping NodeToFace node to face mapping -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-