LumpedMassEADBuilder Class¶
-
class
NXOpen.CAE.
LumpedMassEADBuilder
¶ Bases:
NXOpen.Builder
This class provides LumpedMass Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateLumpedMassEadBuilder()
Default values.
Property Value ExpressionMass.Value 1 (millimeters part), 1 (inches part) MassState Apply New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Elements | Returns the select element operator selects elements |
ExpressionMass | Returns the expression mass operator gets LumpedMass mass value |
MassState | Returns or sets the mass state drives action upon commit |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LumpedMassEADBuilderState Enumeration | indicates to apply or clear the mass property upon commit |
Property Detail¶
Elements¶
-
LumpedMassEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ExpressionMass¶
-
LumpedMassEADBuilder.
ExpressionMass
¶ Returns the expression mass operator gets LumpedMass mass value
-------------------------------------
Getter Method
Signature
ExpressionMass
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MassState¶
-
LumpedMassEADBuilder.
MassState
¶ Returns or sets the mass state drives action upon commit
-------------------------------------
Getter Method
Signature
MassState
Returns: Return type: NXOpen.CAE.LumpedMassEADBuilderState
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
MassState
Parameters: massState ( NXOpen.CAE.LumpedMassEADBuilderState
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
LumpedMassEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.