LbcAssociationMgrBcType Enumeration¶
NXOpen.CAE.LbcAssociationMgr.BcType is an alias for NXOpen.CAE.LbcAssociationMgrBcType
-
class
NXOpen.CAE.
LbcAssociationMgrBcType
¶ Bases:
object
Option to associate bc type, load, constraint or simulation objects
Enum Members
Enum Member Enum Member Description Load Associate loads Constraint Associate constraints SimulationObject Associate simulation objects NotSet no valid type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-