LayoutStateCollection Class¶
-
class
NXOpen.CAE.
LayoutStateCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.LayoutState
.To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CloneLayoutState | Clones the specified NXOpen.CAE.LayoutState |
CreateEmptyLayoutState | Creates an empty NXOpen.CAE.LayoutState |
CreateLayoutStateApplicator | Creates a NXOpen.CAE.LayoutStateApplicator . |
CreateLayoutStateBuilder | Creates a NXOpen.CAE.LayoutStateBuilder . |
DeleteLayoutState | Deletes the specified NXOpen.CAE.LayoutState |
Find | Finds a NXOpen.CAE.LayoutState with the specified name. |
Method Detail¶
CloneLayoutState¶
-
LayoutStateCollection.
CloneLayoutState
¶ Clones the specified
NXOpen.CAE.LayoutState
Signature
CloneLayoutState(fromLayoutState, newName)
Parameters: - fromLayoutState (
NXOpen.CAE.LayoutState
) – cloned layout state - newName (str) – name of the new layout state
Returns: resulting layout state
Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- fromLayoutState (
CreateEmptyLayoutState¶
-
LayoutStateCollection.
CreateEmptyLayoutState
¶ Creates an empty
NXOpen.CAE.LayoutState
Signature
CreateEmptyLayoutState(layoutStateName)
Parameters: layoutStateName (str) – name of the new layout state Returns: resulting layout state Return type: NXOpen.CAE.LayoutState
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateLayoutStateApplicator¶
-
LayoutStateCollection.
CreateLayoutStateApplicator
¶ Creates a
NXOpen.CAE.LayoutStateApplicator
.This builder is used to visualize layout states or exported layout states.
Signature
CreateLayoutStateApplicator()
Returns: Return type: NXOpen.CAE.LayoutStateApplicator
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateLayoutStateBuilder¶
-
LayoutStateCollection.
CreateLayoutStateBuilder
¶ Creates a
NXOpen.CAE.LayoutStateBuilder
.This builder is used to create or edit Layout States.
Signature
CreateLayoutStateBuilder(layoutState)
Parameters: layoutState ( NXOpen.CAE.LayoutState
) –Returns: Return type: NXOpen.CAE.LayoutStateBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteLayoutState¶
-
LayoutStateCollection.
DeleteLayoutState
¶ Deletes the specified
NXOpen.CAE.LayoutState
Signature
DeleteLayoutState(layoutState)
Parameters: layoutState ( NXOpen.CAE.LayoutState
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Find¶
-
LayoutStateCollection.
Find
¶ Finds a
NXOpen.CAE.LayoutState
with the specified name.Signature
Find(name)
Parameters: name (str) – name of the layout state Returns: Return type: NXOpen.CAE.LayoutState
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)