LaminateViewDrapingResultsBuilderOuputChoice Enumeration

NXOpen.CAE.LaminateViewDrapingResultsBuilder.OuputChoice is an alias for NXOpen.CAE.LaminateViewDrapingResultsBuilderOuputChoice

class NXOpen.CAE.LaminateViewDrapingResultsBuilderOuputChoice

Bases: object

Represents output choice

Enum Members

Enum Member Enum Member Description
Spreadsheet
Csv
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.