LaminateSpreadsheetReportBuilderSortingType Enumeration¶
NXOpen.CAE.LaminateSpreadsheetReportBuilder.SortingType is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderSortingType
-
class
NXOpen.CAE.
LaminateSpreadsheetReportBuilderSortingType
¶ Bases:
object
Sorting rule for the spreadsheet post report
Enum Members
Enum Member Enum Member Description ElementId Sort results using the element id PlyId Sort results using the ply id StressXX Sort results using the stress XX component StressYY Sort results using the stress YY component StressZZ Sort results using the stress ZZ component StressXY Sort results using the stress XY component StressZX Sort results using the stress ZX component StressYZ Sort results using the stress YZ component StressMaxP Sort results using the maximum principal stress StressMinP Sort results using the minimum principal stress StressMaxS Sort results using the maximum shear stress StrainXX Sort results using the strain XX component StrainYY Sort results using the strain XX component StrainZZ Sort results using the strain XX component StrainXY Sort results using the strain XX component StrainZX Sort results using the strain XX component StrainYZ Sort results using the strain XX component StrainMaxP Sort results using the maximum principal strain StrainMinP Sort results using the minimum principal strain StrainMaxS Sort results using the maximum shear strain PlyFailureIndex Sort results based on the ply failure index PlyStrengthRatio Sort results based on the ply strength ratio PlyMarginofSafety Sort results based on the ply margin of safety BondFailureIndex Sort results based on the bonding failure index BondStrengthRatio Sort results based on the bonding strength ratio BondMarginofSafety Sort results based on the bonding margin of safety -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-