LaminateSpreadsheetReportBuilderFilteringType Enumeration¶
NXOpen.CAE.LaminateSpreadsheetReportBuilder.FilteringType is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderFilteringType
-
class
NXOpen.CAE.
LaminateSpreadsheetReportBuilderFilteringType
¶ Bases:
object
Filtering rule for the spreadsheet post report
Enum Members
Enum Member Enum Member Description NotSet Don’t filter any values StressXX Filter values based on Stress XX component StressYY Filter values based on Stress YY component StressZZ Filter values based on Stress ZZ component StressXY Filter values based on Stress XY component StressZX Filter values based on Stress ZX component StressYZ Filter values based on Stress YZ component StressMaxP Filter values based on the maximum principal stress StressMinP Filter values based on the minimum principal stress StressMaxS Filter values based on the maximum shear stress StrainXX Filter values based on Strain XX component StrainYY Filter values based on Strain YY component StrainZZ Filter values based on Strain ZZ component StrainXY Filter values based on Strain XY component StrainZX Filter values based on Strain ZX component StrainYZ Filter values based on Strain YZ component StrainMaxP Filter values based on the maximum principal strain StrainMinP Filter values based on the minimum principal strain StrainMaxS Filter values based on the maximum shear strain PlyFailureIndex Filter values based on the ply failure index PlyStrengthRatio Filter values based on the ply strength ratio PlyMarginofSafety Filter values based on the ply margin of safety BondFailureIndex Filter values based on the bonding failure index BondStrengthRatio Filter values based on the bonding strength ratio BondMarginofSafety Filter values based on the bonding margin of safety -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-