LaminateSineEventBuilderAdditionalFrequeciesUnitsEnum Enumeration

NXOpen.CAE.LaminateSineEventBuilder.AdditionalFrequeciesUnitsEnum is an alias for NXOpen.CAE.LaminateSineEventBuilderAdditionalFrequeciesUnitsEnum

class NXOpen.CAE.LaminateSineEventBuilderAdditionalFrequeciesUnitsEnum

Bases: object

The additional frequencies units

Enum Members

Enum Member Enum Member Description
Hz
KHz
MHz
GHz
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.