LaminatePostReportCollection Class¶
-
class
NXOpen.CAE.
LaminatePostReportCollection
¶ Bases:
object
Represents a collection of laminate post reports
To obtain an instance of this class, refer to
NXOpen.CAE.LaminateManager
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ActivePostReport | Returns or sets the active laminate post report |
Methods¶
Method | Description |
---|---|
ClonePostReport | Clones the laminate post report |
CreateLaminateGraphicalReportBuilder | Creates the builder for the NXOpen.CAE.LaminateGraphicalReport class |
CreateLaminatePostReportBuilder | Creates the builder for the NXOpen.CAE.LaminatePostReport class |
CreateLaminateQuickReportBuilder | Creates the builder for the NXOpen.CAE.LaminateQuickReport class |
CreateLaminateSpreadsheetReportBuilder | Creates the builder for the NXOpen.CAE.LaminateSpreadsheetReport class |
DeletePostReport | Deletes the laminate post report |
FindObject | Finds a laminate post report with the specified name |
Property Detail¶
ActivePostReport¶
-
LaminatePostReportCollection.
ActivePostReport
¶ Returns or sets the active laminate post report
-------------------------------------
Getter Method
Signature
ActivePostReport
Returns: Active laminate post report Return type: NXOpen.CAE.LaminatePostReport
New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
-------------------------------------
Setter Method
Signature
ActivePostReport
Parameters: postReport ( NXOpen.CAE.LaminatePostReport
) – Laminate post report to be set activeNew in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Method Detail¶
ClonePostReport¶
-
LaminatePostReportCollection.
ClonePostReport
¶ Clones the laminate post report
Signature
ClonePostReport(postReport)
Parameters: postReport ( NXOpen.CAE.LaminatePostReport
) – Laminate post report to be clonedNew in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
CreateLaminateGraphicalReportBuilder¶
-
LaminatePostReportCollection.
CreateLaminateGraphicalReportBuilder
¶ Creates the builder for the
NXOpen.CAE.LaminateGraphicalReport
classSignature
CreateLaminateGraphicalReportBuilder(graphicalReport)
Parameters: graphicalReport – Graphical Report being edited. Not needed in creation mode. :type graphicalReport:
NXOpen.CAE.LaminateGraphicalReport
:returns: Laminate Graphical Report builder :rtype:NXOpen.CAE.LaminateGraphicalReportBuilder
New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
CreateLaminatePostReportBuilder¶
-
LaminatePostReportCollection.
CreateLaminatePostReportBuilder
¶ Creates the builder for the
NXOpen.CAE.LaminatePostReport
classSignature
CreateLaminatePostReportBuilder(postReport)
Parameters: postReport – Post Report being edited. Not needed in creation mode. :type postReport:
NXOpen.CAE.LaminatePostReport
:returns: Laminate Post Report builder :rtype:NXOpen.CAE.LaminatePostReportBuilder
New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
CreateLaminateQuickReportBuilder¶
-
LaminatePostReportCollection.
CreateLaminateQuickReportBuilder
¶ Creates the builder for the
NXOpen.CAE.LaminateQuickReport
classSignature
CreateLaminateQuickReportBuilder(quickReport)
Parameters: quickReport – Quick Report being edited. Not needed in creation mode. :type quickReport:
NXOpen.CAE.LaminateQuickReport
:returns: Laminate Quick Report builder :rtype:NXOpen.CAE.LaminateQuickReportBuilder
New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateLaminateSpreadsheetReportBuilder¶
-
LaminatePostReportCollection.
CreateLaminateSpreadsheetReportBuilder
¶ Creates the builder for the
NXOpen.CAE.LaminateSpreadsheetReport
classSignature
CreateLaminateSpreadsheetReportBuilder(spreadsheetReport)
Parameters: spreadsheetReport – Spreadsheet Report being edited. Not needed in creation mode. :type spreadsheetReport:
NXOpen.CAE.LaminateSpreadsheetReport
:returns: Laminate Spreadsheet Report builder :rtype:NXOpen.CAE.LaminateSpreadsheetReportBuilder
New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
DeletePostReport¶
-
LaminatePostReportCollection.
DeletePostReport
¶ Deletes the laminate post report
Signature
DeletePostReport(postReport)
Parameters: postReport ( NXOpen.CAE.LaminatePostReport
) – Laminate post report to be deletedNew in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
FindObject¶
-
LaminatePostReportCollection.
FindObject
¶ Finds a laminate post report with the specified name
Signature
FindObject(name)
Parameters: name (str) – Laminate Post Report name to be found Returns: Laminate Post Report found Return type: NXOpen.CAE.LaminatePostReport
New in version NX8.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)