LaminatePlyPlyFailureTheoryType Enumeration¶
NXOpen.CAE.LaminatePly.PlyFailureTheoryType is an alias for NXOpen.CAE.LaminatePlyPlyFailureTheoryType
-
class
NXOpen.CAE.
LaminatePlyPlyFailureTheoryType
¶ Bases:
object
Ply failure theory types
Enum Members
Enum Member Enum Member Description NotSet No failure theory selected Hill Hill failure criteria Hoffman Hoffman failure criteria TsaiWu Tsai-Wu failure criteria MaxStrain Maximum Strain failure criteria MaxStress Maximum Stress failure criteria MaxTransverseShear Maximum Transverse Shear Stress failure criteria VonMisesYield Von Mises Yield failure criteria VonMisesUltimate Von Mises Utlimate failure criteria ProgressiveFailure Progressive Failure failure criteria UserDefined User defined ply failure theory (thru a user dll) -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-