LaminatePlyInterLaminarFailureTheoryType Enumeration¶
NXOpen.CAE.LaminatePly.InterLaminarFailureTheoryType is an alias for NXOpen.CAE.LaminatePlyInterLaminarFailureTheoryType
-
class
NXOpen.CAE.
LaminatePlyInterLaminarFailureTheoryType
¶ Bases:
object
Inter-Laminar failure theory types
Enum Members
Enum Member Enum Member Description NotSet No failure theory selected TransverseShearStress Transverse Shear Stress inter-laminar failure criteria NormalStress Normal Stress inter-laminar failure criteria UserDefined User defined interlaminar failure theory (thru a user dll) -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-