LaminateMatOrientationCollection Class¶
-
class
NXOpen.CAE.
LaminateMatOrientationCollection
¶ Bases:
object
Represents a collection of layup growth rules
To obtain an instance of this class, refer to
NXOpen.CAE.LaminateGlobalLayupMgr
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.CAE.LaminateMatOrientation with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
LaminateMatOrientationCollection.
FindObject
¶ Finds the
NXOpen.CAE.LaminateMatOrientation
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: material orientation found Return type: NXOpen.CAE.LaminateMatOrientation
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)