LaminateImportedLayupBuilderFileEnum Enumeration¶
NXOpen.CAE.LaminateImportedLayupBuilder.FileEnum is an alias for NXOpen.CAE.LaminateImportedLayupBuilderFileEnum
-
class
NXOpen.CAE.
LaminateImportedLayupBuilderFileEnum
¶ Bases:
object
Type of external file to be imported. Only FiberSim layup XML file supported for now.
Enum Members
Enum Member Enum Member Description FiberSimXml FiberSIM layup XML file. FiberSimH5 FiberSIM layup HDF5 file. SimulaytLayup Simulayt Layup File. FiberSimPart Use the FiberSim data in the current part CatiaPlyGroups CATIA Ply Groups. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-