LaminateGraphicalReportBuilderPlyExportOptionType Enumeration¶
NXOpen.CAE.LaminateGraphicalReportBuilder.PlyExportOptionType is an alias for NXOpen.CAE.LaminateGraphicalReportBuilderPlyExportOptionType
-
class
NXOpen.CAE.
LaminateGraphicalReportBuilderPlyExportOptionType
¶ Bases:
object
Ply export options. With or without ply ids.
Enum Members
Enum Member Enum Member Description GlobalPlyId Export the ply global ids to the bun file Layer Export plies as layers -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-