LaminateGraphicalReportBuilderFailureModeType Enumeration¶
NXOpen.CAE.LaminateGraphicalReportBuilder.FailureModeType is an alias for NXOpen.CAE.LaminateGraphicalReportBuilderFailureModeType
-
class
NXOpen.CAE.
LaminateGraphicalReportBuilderFailureModeType
¶ Bases:
object
Failure indices mode. NXLC can compute in-plane ply failure indices and/or interlaminar failure indices
Enum Members
Enum Member Enum Member Description InPlanePly Ply failure index Interlaminar Bonding failure index Both Both failure index type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-