LaminateGlobalLayupStackingRecipeType Enumeration¶
NXOpen.CAE.LaminateGlobalLayup.StackingRecipeType is an alias for NXOpen.CAE.LaminateGlobalLayupStackingRecipeType
-
class
NXOpen.CAE.
LaminateGlobalLayupStackingRecipeType
¶ Bases:
object
Used to specify the stacking recipe of the global layup
Enum Members
Enum Member Enum Member Description Normal Normal Symmetric Symmetric SymmetricWithCore Symmetric with core Repeated Repeated RepeatedWithCore Repeated with core -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-