LaminateFillSetupBuilder Class¶
-
class
NXOpen.CAE.
LaminateFillSetupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateFillSetupBuilder
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateLaminateFillSetupBuilder()
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
FillName | Returns or sets the name of the laminate fill setup |
HomogeneousPlies | Returns or sets the option to (de)activate homogeneous ply meshes |
LimitThicknessVariation | Returns or sets the layup thickness variation control option |
SamcefElementType | Returns or sets the samcef element type |
SamcefSolidShells | Returns or sets the option to use SAMCEF solid shells |
Selection | Returns the face(s) on which to perform the fill |
SinglePlyPerLayer | Returns or sets the option to group plies into single layer(s) of extruded elements |
Tag | Returns the Tag for this object. |
ThicknessVariationDownLimit | Returns or sets the global maximum allowed relative thickness reduction variation, in percentage |
ThicknessVariationUpLimit | Returns or sets the global maximum allowed relative thickness increase variation, in percentage |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateFillSetupBuilderSamcefElementTypeEnum Enumeration | Samcef element type. |
Property Detail¶
FillName¶
-
LaminateFillSetupBuilder.
FillName
¶ Returns or sets the name of the laminate fill setup
-------------------------------------
Getter Method
Signature
FillName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FillName
Parameters: fillName (str) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
HomogeneousPlies¶
-
LaminateFillSetupBuilder.
HomogeneousPlies
¶ Returns or sets the option to (de)activate homogeneous ply meshes
-------------------------------------
Getter Method
Signature
HomogeneousPlies
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomogeneousPlies
Parameters: homogeneousPlies (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
LimitThicknessVariation¶
-
LaminateFillSetupBuilder.
LimitThicknessVariation
¶ Returns or sets the layup thickness variation control option
-------------------------------------
Getter Method
Signature
LimitThicknessVariation
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitThicknessVariation
Parameters: limitThicknessVariation (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SamcefElementType¶
-
LaminateFillSetupBuilder.
SamcefElementType
¶ Returns or sets the samcef element type
-------------------------------------
Getter Method
Signature
SamcefElementType
Returns: Return type: NXOpen.CAE.LaminateFillSetupBuilderSamcefElementTypeEnum
New in version NX12.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
-------------------------------------
Setter Method
Signature
SamcefElementType
Parameters: samcefElementType ( NXOpen.CAE.LaminateFillSetupBuilderSamcefElementTypeEnum
) –New in version NX12.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SamcefSolidShells¶
-
LaminateFillSetupBuilder.
SamcefSolidShells
¶ Returns or sets the option to use SAMCEF solid shells
-------------------------------------
Getter Method
Signature
SamcefSolidShells
Returns: Return type: bool New in version NX10.0.0.
Deprecated since version NX12.0.0: Use method
NXOpen.CAE.LaminateFillSetupBuilder.SamcefElementType()
License requirements: None.
-------------------------------------
Setter Method
Signature
SamcefSolidShells
Parameters: samcefSolidShells (bool) – New in version NX10.0.0.
Deprecated since version NX12.0.0: Use method
NXOpen.CAE.LaminateFillSetupBuilder.SetSamcefElementType()
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Selection¶
-
LaminateFillSetupBuilder.
Selection
¶ Returns the face(s) on which to perform the fill
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.CAE.LaminateSelectEntitiesBuilder
New in version NX7.5.2.
License requirements: None.
SinglePlyPerLayer¶
-
LaminateFillSetupBuilder.
SinglePlyPerLayer
¶ Returns or sets the option to group plies into single layer(s) of extruded elements
-------------------------------------
Getter Method
Signature
SinglePlyPerLayer
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SinglePlyPerLayer
Parameters: singlePlyPerLayer (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ThicknessVariationDownLimit¶
-
LaminateFillSetupBuilder.
ThicknessVariationDownLimit
¶ Returns or sets the global maximum allowed relative thickness reduction variation, in percentage
-------------------------------------
Getter Method
Signature
ThicknessVariationDownLimit
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessVariationDownLimit
Parameters: thicknessVariationDownLimit (float) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ThicknessVariationUpLimit¶
-
LaminateFillSetupBuilder.
ThicknessVariationUpLimit
¶ Returns or sets the global maximum allowed relative thickness increase variation, in percentage
-------------------------------------
Getter Method
Signature
ThicknessVariationUpLimit
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessVariationUpLimit
Parameters: thicknessVariationUpLimit (float) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
Validate¶
-
LaminateFillSetupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.