LaminateExtrudeSetupCollection Class¶
-
class
NXOpen.CAE.
LaminateExtrudeSetupCollection
¶ Bases:
object
Represents a collection of laminate extrusion setups
To obtain an instance of this class, refer to
NXOpen.CAE.LaminateGlobalLayupMgr
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.CAE.LaminateExtrudeSetup with the given identifier as recorded in a journal. |
RemoveExtrudeSetup | Remove and delete an NXOpen.CAE.LaminateExtrudeSetup from the model |
Method Detail¶
FindObject¶
-
LaminateExtrudeSetupCollection.
FindObject
¶ Finds the
NXOpen.CAE.LaminateExtrudeSetup
with the given identifier as recorded in a journal.Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Corresponding extrusion setup found Return type: NXOpen.CAE.LaminateExtrudeSetup
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
RemoveExtrudeSetup¶
-
LaminateExtrudeSetupCollection.
RemoveExtrudeSetup
¶ Remove and delete an
NXOpen.CAE.LaminateExtrudeSetup
from the modelSignature
RemoveExtrudeSetup(setup)
Parameters: setup ( NXOpen.CAE.LaminateExtrudeSetup
) – The extrusion setup to removeNew in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)