LaminateExtrudeSetupBuilder Class¶
-
class
NXOpen.CAE.
LaminateExtrudeSetupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateExtrudeSetup
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateLaminateExtrudeSetupBuilder()
Default values.
Property Value CutFaceDrops 0 FlipNormals 0 KeepInvalidElems 0 MinElemThickness 0.05 NumSmoothIterations 2 SinglePlyPerLayer 1 SmoothNormals 0 SmoothRatio 0.5 New in version NX6.0.4.
Properties¶
Property | Description |
---|---|
CutFaceDrops | Returns or sets the option to consider cut ply elements as drop-offs |
CutFaceSelect | Returns the cutting face(s) selection |
Cuts | Returns or sets the option use cutting faces |
ExtrudeName | Returns or sets the name of the laminate extrusion setup |
FlipNormals | Returns or sets the option to flip the element normals for the extrusion process |
HomogeneousPlies | Returns or sets the option to (de)activate homogeneous ply meshes |
KeepInvalidElems | Returns or sets the option to keep invalid extruded elements |
MinElemThickness | Returns or sets the relative minimum thickness for a corner node ply element. |
NumSmoothIterations | Returns or sets the number of iterations for normal smoothing |
ReferencePlaneLocation | Returns or sets the option to (de)activate reference plane location |
SamcefElementType | Returns or sets the samcef element type |
SamcefSolidShells | Returns or sets the option to use SAMCEF solid shells |
SandwichBottomSkinMeshOption | Returns or sets the bottom-skin-mesh options for the sandwich inflation |
SandwichInflation | Returns or sets the option to (de)activate the sandwich inflatoin |
SandwichNumCoreElementLayers | Returns or sets the number of core element layers for the sandwich inflation |
SandwichTopSkinMeshOption | Returns or sets the top-skin-mesh options for the sandwich inflation |
Selection | Returns the geometric face(s) and element faces on which to perform the extrusion |
SinglePlyPerLayer | Returns or sets the option to group plies into single layer(s) of extruded elements |
SmoothNormals | Returns or sets the option to smooth the shell normals used for extrusion |
SmoothRatio | Returns or sets the neighbor normal weigth ratio for normal smoothing |
SnapToCutFaceTolerance | Returns the tolerance to snap nodes to the cutting face borders. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateExtrudeSetupBuilderSamcefElementTypeEnum Enumeration | Samcef element type. |
Property Detail¶
CutFaceDrops¶
-
LaminateExtrudeSetupBuilder.
CutFaceDrops
¶ Returns or sets the option to consider cut ply elements as drop-offs
-------------------------------------
Getter Method
Signature
CutFaceDrops
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutFaceDrops
Parameters: cutFaceDrops (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CutFaceSelect¶
-
LaminateExtrudeSetupBuilder.
CutFaceSelect
¶ Returns the cutting face(s) selection
-------------------------------------
Getter Method
Signature
CutFaceSelect
Returns: Return type: NXOpen.CAE.SelectCAEFaceList
New in version NX9.0.0.
License requirements: None.
Cuts¶
-
LaminateExtrudeSetupBuilder.
Cuts
¶ Returns or sets the option use cutting faces
-------------------------------------
Getter Method
Signature
Cuts
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Cuts
Parameters: cuts (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ExtrudeName¶
-
LaminateExtrudeSetupBuilder.
ExtrudeName
¶ Returns or sets the name of the laminate extrusion setup
-------------------------------------
Getter Method
Signature
ExtrudeName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtrudeName
Parameters: extrudeName (str) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FlipNormals¶
-
LaminateExtrudeSetupBuilder.
FlipNormals
¶ Returns or sets the option to flip the element normals for the extrusion process
-------------------------------------
Getter Method
Signature
FlipNormals
Returns: Return type: bool New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipNormals
Parameters: flipNormals (bool) – New in version NX6.0.4.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
HomogeneousPlies¶
-
LaminateExtrudeSetupBuilder.
HomogeneousPlies
¶ Returns or sets the option to (de)activate homogeneous ply meshes
-------------------------------------
Getter Method
Signature
HomogeneousPlies
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomogeneousPlies
Parameters: homogeneousPlies (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
KeepInvalidElems¶
-
LaminateExtrudeSetupBuilder.
KeepInvalidElems
¶ Returns or sets the option to keep invalid extruded elements
-------------------------------------
Getter Method
Signature
KeepInvalidElems
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepInvalidElems
Parameters: keepInvalidElems (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
MinElemThickness¶
-
LaminateExtrudeSetupBuilder.
MinElemThickness
¶ Returns or sets the relative minimum thickness for a corner node ply element.
-------------------------------------
Getter Method
Signature
MinElemThickness
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinElemThickness
Parameters: minElemThickness (float) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NumSmoothIterations¶
-
LaminateExtrudeSetupBuilder.
NumSmoothIterations
¶ Returns or sets the number of iterations for normal smoothing
-------------------------------------
Getter Method
Signature
NumSmoothIterations
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumSmoothIterations
Parameters: numSmoothIterations (int) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ReferencePlaneLocation¶
-
LaminateExtrudeSetupBuilder.
ReferencePlaneLocation
¶ Returns or sets the option to (de)activate reference plane location
-------------------------------------
Getter Method
Signature
ReferencePlaneLocation
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePlaneLocation
Parameters: referencePlaneLocation (bool) – New in version NX11.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SamcefElementType¶
-
LaminateExtrudeSetupBuilder.
SamcefElementType
¶ Returns or sets the samcef element type
-------------------------------------
Getter Method
Signature
SamcefElementType
Returns: Return type: NXOpen.CAE.LaminateExtrudeSetupBuilderSamcefElementTypeEnum
New in version NX12.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
-------------------------------------
Setter Method
Signature
SamcefElementType
Parameters: samcefElementType ( NXOpen.CAE.LaminateExtrudeSetupBuilderSamcefElementTypeEnum
) –New in version NX12.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SamcefSolidShells¶
-
LaminateExtrudeSetupBuilder.
SamcefSolidShells
¶ Returns or sets the option to use SAMCEF solid shells
-------------------------------------
Getter Method
Signature
SamcefSolidShells
Returns: Return type: bool New in version NX10.0.0.
Deprecated since version NX12.0.0: Use method
NXOpen.CAE.LaminateExtrudeSetupBuilder.SamcefElementType()
License requirements: None.
-------------------------------------
Setter Method
Signature
SamcefSolidShells
Parameters: samcefSolidShells (bool) – New in version NX10.0.0.
Deprecated since version NX12.0.0: Use method
NXOpen.CAE.LaminateExtrudeSetupBuilder.SetSamcefElementType()
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SandwichBottomSkinMeshOption¶
-
LaminateExtrudeSetupBuilder.
SandwichBottomSkinMeshOption
¶ Returns or sets the bottom-skin-mesh options for the sandwich inflation
-------------------------------------
Getter Method
Signature
SandwichBottomSkinMeshOption
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SandwichBottomSkinMeshOption
Parameters: sandwichBottomSkinMeshOption (int) – New in version NX11.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SandwichInflation¶
-
LaminateExtrudeSetupBuilder.
SandwichInflation
¶ Returns or sets the option to (de)activate the sandwich inflatoin
-------------------------------------
Getter Method
Signature
SandwichInflation
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SandwichInflation
Parameters: sandwichInflation (bool) – New in version NX11.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SandwichNumCoreElementLayers¶
-
LaminateExtrudeSetupBuilder.
SandwichNumCoreElementLayers
¶ Returns or sets the number of core element layers for the sandwich inflation
-------------------------------------
Getter Method
Signature
SandwichNumCoreElementLayers
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SandwichNumCoreElementLayers
Parameters: sandwichNumCoreElementLayers (int) – New in version NX11.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SandwichTopSkinMeshOption¶
-
LaminateExtrudeSetupBuilder.
SandwichTopSkinMeshOption
¶ Returns or sets the top-skin-mesh options for the sandwich inflation
-------------------------------------
Getter Method
Signature
SandwichTopSkinMeshOption
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SandwichTopSkinMeshOption
Parameters: sandwichTopSkinMeshOption (int) – New in version NX11.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Selection¶
-
LaminateExtrudeSetupBuilder.
Selection
¶ Returns the geometric face(s) and element faces on which to perform the extrusion
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.CAE.LaminateSelectEntitiesBuilder
New in version NX7.5.2.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SinglePlyPerLayer¶
-
LaminateExtrudeSetupBuilder.
SinglePlyPerLayer
¶ Returns or sets the option to group plies into single layer(s) of extruded elements
-------------------------------------
Getter Method
Signature
SinglePlyPerLayer
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SinglePlyPerLayer
Parameters: singlePlyPerLayer (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SmoothNormals¶
-
LaminateExtrudeSetupBuilder.
SmoothNormals
¶ Returns or sets the option to smooth the shell normals used for extrusion
-------------------------------------
Getter Method
Signature
SmoothNormals
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothNormals
Parameters: smoothNormals (bool) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SmoothRatio¶
-
LaminateExtrudeSetupBuilder.
SmoothRatio
¶ Returns or sets the neighbor normal weigth ratio for normal smoothing
-------------------------------------
Getter Method
Signature
SmoothRatio
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothRatio
Parameters: smoothRatio (float) – New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SnapToCutFaceTolerance¶
-
LaminateExtrudeSetupBuilder.
SnapToCutFaceTolerance
¶ Returns the tolerance to snap nodes to the cutting face borders.
-------------------------------------
Getter Method
Signature
SnapToCutFaceTolerance
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LaminateExtrudeSetupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.