IMeshManager Class¶
-
class
NXOpen.CAE.
IMeshManager
¶ Bases:
NXOpen.TaggedObject
Manages meshes:py:class:NXOpen.CAE.IMeshManager in cae parts
This is an abstract class, and cannot be created.
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.CAE.Mesh with the given identifier as recorded in a journal. |
GetElementStatus | Returns the elements status for this manager |
GetMeshCollectors | Returns the IMeshCollectors NXOpen.CAE.IMeshCollector for this manager |
GetMeshes | Returns the Meshes NXOpen.CAE.Mesh for this manager |
GetNodeStatus | Returns the node status for this manager |
Structs¶
IMeshManagerStatusInfo_Struct Struct | Contains status information |
Method Detail¶
FindObject¶
-
IMeshManager.
FindObject
¶ Finds the
NXOpen.CAE.Mesh
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Mesh or collector name Returns: mesh or collector with this identifier Return type: NXOpen.TaggedObject
New in version NX3.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetElementStatus¶
-
IMeshManager.
GetElementStatus
¶ Returns the elements status for this manager
Signature
GetElementStatus()
Returns: Return type: NXOpen.CAE.IMeshManagerStatusInfo_Struct
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMeshCollectors¶
-
IMeshManager.
GetMeshCollectors
¶ Returns the IMeshCollectors
NXOpen.CAE.IMeshCollector
for this managerSignature
GetMeshCollectors()
Returns: Return type: list of NXOpen.CAE.IMeshCollector
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetMeshes¶
-
IMeshManager.
GetMeshes
¶ Returns the Meshes
NXOpen.CAE.Mesh
for this managerSignature
GetMeshes()
Returns: Return type: list of NXOpen.CAE.Mesh
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetNodeStatus¶
-
IMeshManager.
GetNodeStatus
¶ Returns the node status for this manager
Signature
GetNodeStatus()
Returns: Return type: NXOpen.CAE.IMeshManagerStatusInfo_Struct
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)