GroupMethod Class¶
-
class
NXOpen.CAE.
GroupMethod
¶ Bases:
NXOpen.SelectionMethod
Represents the output from the Group smart selector method
To obtain an instance of this class use CAE::SmartSelectionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetEntities | Returns the resultant entities |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
Method Detail¶
Dispose¶
-
GroupMethod.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetEntities¶
-
GroupMethod.
GetEntities
¶ Returns the resultant entities
Signature
GetEntities()
Returns: Resultant entities Return type: list of NXOpen.TaggedObject
New in version NX6.0.4.
License requirements: None.