GroupEdgeMethod Class¶
-
class
NXOpen.CAE.
GroupEdgeMethod
¶ Bases:
NXOpen.SelectionMethod
Represents the output from the Group Edge smart selector method
To obtain an instance of this class use CAE::SmartSelectionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetEdges | Returns the resultant edges |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
Method Detail¶
Dispose¶
-
GroupEdgeMethod.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetEdges¶
-
GroupEdgeMethod.
GetEdges
¶ Returns the resultant edges
Signature
GetEdges()
Returns: Resultant edges Return type: list of NXOpen.CAE.CAEEdge
New in version NX11.0.0.
License requirements: None.