GroupByBoundaryBuilder Class¶
-
class
NXOpen.CAE.
GroupByBoundaryBuilder
¶ Bases:
NXOpen.Builder
Represents a
CAE.GroupByBoundaryBuilder
.To create a new instance of this class, use
NXOpen.CAE.CaeGroupCollection.CreateGroupByBoundaryBuilder()
New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
ClosedVolumeToggle | Returns or sets the closed volume option |
CreateTwoGroups | Returns or sets the first selection group |
NormalDirectionFlipped | Returns or sets the normal direction flipped |
SeedElement | Returns or sets the seed element |
SelectElementsGroupOne | Returns the elements in group one |
SelectElementsGroupTwo | Returns the elements in group two |
SelectRemovedGroup | Returns the elements removed as ribs |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindVolume | Finds a selection of elements representing a volume based on the chosen seed element |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ClosedVolumeToggle¶
-
GroupByBoundaryBuilder.
ClosedVolumeToggle
¶ Returns or sets the closed volume option
-------------------------------------
Getter Method
Signature
ClosedVolumeToggle
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClosedVolumeToggle
Parameters: toggle1 (bool) – New in version NX11.0.0.
License requirements: None.
CreateTwoGroups¶
-
GroupByBoundaryBuilder.
CreateTwoGroups
¶ Returns or sets the first selection group
-------------------------------------
Getter Method
Signature
CreateTwoGroups
Returns: Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateTwoGroups
Parameters: direction0 (bool) – New in version NX10.0.2.
License requirements: None.
NormalDirectionFlipped¶
-
GroupByBoundaryBuilder.
NormalDirectionFlipped
¶ Returns or sets the normal direction flipped
-------------------------------------
Getter Method
Signature
NormalDirectionFlipped
Returns: Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalDirectionFlipped
Parameters: toggle0 (bool) – New in version NX10.0.2.
License requirements: None.
SeedElement¶
-
GroupByBoundaryBuilder.
SeedElement
¶ Returns or sets the seed element
-------------------------------------
Getter Method
Signature
SeedElement
Returns: Return type: NXOpen.CAE.FEElement
New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedElement
Parameters: seedElement ( NXOpen.CAE.FEElement
) –New in version NX10.0.2.
License requirements: None.
SelectElementsGroupOne¶
-
GroupByBoundaryBuilder.
SelectElementsGroupOne
¶ Returns the elements in group one
-------------------------------------
Getter Method
Signature
SelectElementsGroupOne
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX10.0.2.
License requirements: None.
SelectElementsGroupTwo¶
-
GroupByBoundaryBuilder.
SelectElementsGroupTwo
¶ Returns the elements in group two
-------------------------------------
Getter Method
Signature
SelectElementsGroupTwo
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX10.0.2.
License requirements: None.
SelectRemovedGroup¶
-
GroupByBoundaryBuilder.
SelectRemovedGroup
¶ Returns the elements removed as ribs
-------------------------------------
Getter Method
Signature
SelectRemovedGroup
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX10.0.2.
License requirements: None.
Method Detail¶
FindVolume¶
-
GroupByBoundaryBuilder.
FindVolume
¶ Finds a selection of elements representing a volume based on the chosen seed element
Signature
FindVolume()
New in version NX10.0.2.
License requirements: None.
Validate¶
-
GroupByBoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.