GeometryRecipeCollection Class¶
-
class
NXOpen.CAE.
GeometryRecipeCollection
¶ Bases:
object
Provides methods for managing set
NXOpen.CAE.GeometryRecipe
To obtain an instance of this class, refer to
NXOpen.CAE.PolygonGeometryManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateFreezeGeometryBuilder | Creates a NXOpen.CAE.GeometryRecipeCollection instance. |
FindObject | Finds the NXOpen.CAE.GeometryRecipe with the given identifier as recorded in a journal. |
Method Detail¶
CreateFreezeGeometryBuilder¶
-
GeometryRecipeCollection.
CreateFreezeGeometryBuilder
¶ Creates a
NXOpen.CAE.GeometryRecipeCollection
instance.Signature
CreateFreezeGeometryBuilder(recipe)
Parameters: recipe ( NXOpen.CAE.FreezeGeometryRecipe
) –Returns: Return type: NXOpen.CAE.FreezeGeometryBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
GeometryRecipeCollection.
FindObject
¶ Finds the
NXOpen.CAE.GeometryRecipe
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the Set you want Returns: Return type: NXOpen.CAE.GeometryRecipe
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)