GapEADBuilderOrientationMethod Enumeration¶
NXOpen.CAE.GapEADBuilder.OrientationMethod is an alias for NXOpen.CAE.GapEADBuilderOrientationMethod
-
class
NXOpen.CAE.
GapEADBuilderOrientationMethod
¶ Bases:
object
indicates which orientation method to use
Enum Members
Enum Member Enum Member Description Vector use a vector to orient the element Csystem use a csystem to orient the element Node use a node to orient the element -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-