FunctionInterpolationMethod Enumeration¶
NXOpen.CAE.Function.InterpolationMethod is an alias for NXOpen.CAE.FunctionInterpolationMethod
-
class
NXOpen.CAE.
FunctionInterpolationMethod
¶ Bases:
object
Defines interpolation method for table function to calculate data as input for solver
Enum Members
Enum Member Enum Member Description Cubic Indicates data calculated by cubic interpolation Akima Indicates data calculated by akima interpolation Linear Indicates data calculated by linear interpolation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-