FrfSet Class¶
-
class
NXOpen.CAE.
FrfSet
¶ Bases:
NXOpen.CAE.AlternateFemRepresentationSource
,NXOpen.CAE.IPostScenarioDataSource
This is the class representing a FRF set.
Not support KF.
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
ForceUpdate | Force update of the Alternate Fem Representation Source |
GetFrfStatus | Get the status of a frf. |
GetNumberOfFrfs | Get the number of frfs. |
Rename | Set the name of the Alternate Fem Representation Source |
SetFrfStatus | Modify the status of a frf. |
Enumerations¶
FrfSetMeasure Enumeration | Measure types |
FrfSetNodeComponent Enumeration | Node component types |
Method Detail¶
GetFrfStatus¶
-
FrfSet.
GetFrfStatus
¶ Get the status of a frf.
Signature
GetFrfStatus(inputNode, inputComponent, outputNode, outputComponent, excitation, response)
Parameters: - inputNode (int) – the input node
- inputComponent (
NXOpen.CAE.FrfSetNodeComponent
) – the input node component - outputNode (int) – the output node
- outputComponent (
NXOpen.CAE.FrfSetNodeComponent
) – the output node component - excitation (
NXOpen.CAE.FrfSetMeasure
) – the excitation - response (
NXOpen.CAE.FrfSetMeasure
) – the response
Returns: the status of the frf
Return type: bool
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetNumberOfFrfs¶
-
FrfSet.
GetNumberOfFrfs
¶ Get the number of frfs.
Signature
GetNumberOfFrfs()
Returns: The number of frfs. Return type: int New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetFrfStatus¶
-
FrfSet.
SetFrfStatus
¶ Modify the status of a frf.
Signature
SetFrfStatus(inputNode, inputComponent, outputNode, outputComponent, excitation, response, status)
Parameters: - inputNode (int) – the input node
- inputComponent (
NXOpen.CAE.FrfSetNodeComponent
) – the input node component - outputNode (int) – the output node
- outputComponent (
NXOpen.CAE.FrfSetNodeComponent
) – the output node component - excitation (
NXOpen.CAE.FrfSetMeasure
) – the excitation - response (
NXOpen.CAE.FrfSetMeasure
) – the response - status (bool) – the status of the frf
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)